This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am designing an new project using MSP430FR4133 and a 7-segment LCD . I received an +5V 7-seg LCD. I already ordered the alternative +3V LCD, it will another 7-10 days, in the mean time i want to test my custom hardware. Is it possible to drive a +5V LCD using MSP430FR4133, i am planing to use an level translator (TXB0108PWR) in between LCD and micro controller. is it advisable to do this experiment. Are their any alternative methods or i should abandon this approach and wait for +3V LCD.
Sai,
Since the MSP430 only supports up to 3.6V, you could use an external 5V level translator, but of course using the 3V LCD will be a cleaner solution. I will close the thread.
**Attention** This is a public forum