This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430G2ET: not recognized by Uniflash

Part Number: MSP-EXP430G2ET
Other Parts Discussed in Thread: UNIFLASH, MSP430G2553

I am developing under 64-bit Debian Linux 10.  I have used this Uniflash successfully with MSP432 and TM4C129 Launchpads.  But Uniflash fails to recognize the MSP-EXP430G2ET Launchpad.  With the Launchpad plugged into the USB port, on startup Uniflash fails to detect it, reporting "No debug probes/devices detected".  I get the same result when I try manual detection.  When I go to New Configuration / Choose Your Device and select Category: MSP, I see many MSP430 boards and devices, but the MSP-EXP430G2ET is not on the list.  The MSP430G2553 chip is also not on the list (there are many MSP430F devices, but no MSP430G devices).  I saw this first with Uniflash 5.2.0, but have now upgraded to Uniflash 6.0.0 with the same problem.  I have re-synced the device database and that didn't help.

At present I have no way to program the MSP-EXP430G2ET board.  (mspdebug also fails; I've started a separate thread about that.)

**Attention** This is a public forum