This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hello,
I have one doubt abouth the RF447 MOdule.
I have one 447MHz Module, connected with MSP430FR6972.
I check the "Rf Tx Power Level" in spectrum,
It is showing "-16db".
But I have one Doubt(one simple question) :
Suppose I do not connect the RF Module, with the MSP430 controller(not even program that also) '
And I want to know the "STANDARD RF TX POWER LEVEL", Can I be able to find that?
I am attaching the spec from the DAtasheet :
English Versiion:
CAN ANYONE TELL ME THE STANDARD RF RX POWER LEVEL ( FACTORY SETTING) ?
regards,
Srijit
hi,
I upload the datasheet,
please check it.
srijit.NMT-UM434R1-C Datashort v1.5 [ Nov 27, 2019 ] (1).pdf
In the Datashhet, it is mentioned about "+10" (in one place).
But I am getting confused.
Can you confirm from the datashhet.
Hi
I think you should get the support from https://www.mobile-technologies.com/
If you have any question about MSP430 you can ask here. Thanks
**Attention** This is a public forum