This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2000: How MSP430FR2000 can work in 1M,and current 120uA

Part Number: MSP430FR2000
Other Parts Discussed in Thread: ENERGYTRACE

RUN“”Flashing the LED" example, The default frequency 2M,current should be 240uA according datasheet,but actual 1.1mA,although I config all IO to output ,and out=0;

And then set clock to VLO(10k,SELMS 011),current 0.9mA。

How can config to avtive mode,about 1M,and hope the current about 120uA?

WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
PMMCTL0 = PMMPW; // Open PMM Module
PM5CTL0 &= ~LOCKLPM5; // Clear locked IO Pins
P1DIR = 0xff; // Set P1.1 to output direction
P2DIR = 0xff; // Set P1.1 to output direction
P1OUT = 0x00;
P2OUT = 0x00;

for (;;)
{
volatile unsigned int i; // volatile to prevent optimization

P1OUT ^= 0x02; // Toggle P1.1 using exclusive-OR

i = 10000; // SW Delay
do i--;
while (i != 0);
}

**Attention** This is a public forum