This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: HID Bridge Connected - Waiting for device and Error as Pulse Generation Parameters are invalid

Part Number: EVM430-FR6043

Greetings,

I am getting started with the EVM430-FR6043 for Gas Sensing Purpose. To get started, I am trying to read data over the USS Application based on the Out Of the Box Example. But always the HID Bridge status in the USS application Shows "waiting for device" msg. Also there is continous error generation with the following messages "Pulse Generation Parameters are Invalid" and "The Output Frequency of HSPLL is invalid"

I have even tried to Flash the Image file "MSP430FR6043EVM_USS_Gas_Demo_EVM_v2_0_AFE3v3_02_30_00_01.txt"  ; but still the problem remains the same.

Further details;

The PC Device Manager Shows MSP UART Application and MSP Debug Interface in COM Ports; additionally two HID Devices are also shown.

The on-board LED status of the EVM are as follows

1. D1 - Flashing approx at 5 secs

2. D2 - OFF

3. LED102 - ON

4. LED201 - Always ON

5. LED202 - Blinking at 1 Secs.

All the other jumper configurations are default and the Power Select Switch is aligned to EZFET

Thanks and Regards,

Amit Kotal

**Attention** This is a public forum