Tool/software: Code Composer Studio
Hello,
I want to use CCS for TIDA 00601 Project. Do you have this project. Can you help me about this subject?
Thank You.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I want to use CCS for TIDA 00601 Project. Do you have this project. Can you help me about this subject?
Thank You.
Hello Candan,
Unfortunately, CCS code is not available for this design. You'll need to use IAR or port the code to CCS.
Regards,
James
Thanks Evans.
So,Can you share any documents that It can help to porting project ?
Hello,
There aren't any porting documents outside of the IAR and CCS compiler documentation. The IAR-based library has implemented some of the low-level math functions in assembly code, so you'd need to port them to CCS which would be challenging. Other than that, I don't know of any other resources.
If CCS is absolutely a requirement, then you may want to consider using the Energy Measurement Design Center which supports CCS. I'm assuming you'll need three shunts, so one option is using the F6779A with isolated modulators (you would need to modify the EMDC-generated source code) or using three i2021 devices as the shunt AFEs optically isolated from the host MCU or processor. Both these devices are supported by EMDC. I would expect the effort of this route would be much less than the alternative mentioned above.
Regards,
James
**Attention** This is a public forum