This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR69891: Cannot activate SPI on MSP430FR69891 (UCB0 or UCB1) , no output on CLK and MOSI pins

Part Number: MSP430FR69891
Other Parts Discussed in Thread: MSP430FR5989, MSP430FR5969

Tool/software: Code Composer Studio

I have a circuit with MSP430FR5989 and need to activate 3 SPI module UCBA1, UCB0, UCB1. Started to test UCB0 and UCB1 with pins as follows: UCB0: P1.4, P1.6, P1.7 and UCB1: P3.0 , P3.1, P3.2

The code I have tested is as below. When I run the code I check the pins on oscilloscope and there is no clk signal on CLK pin and no data on SIMO pin (I have checked other pins too)
I have test same code on TI development board with MCU MSP430FR5969. I only change this line for corresponding pins (P2.2, P1.6, P1.7). It works fine on development board. One time I forgot to change P2.2 as clock but it was still working fine with MOSI pin on lauchpad.
GPIO_setAsPeripheralModuleFunctionInputPin(
       GPIO_PORT_P1,
       GPIO_PIN4 + GPIO_PIN6 + GPIO_PIN7,
       GPIO_SECONDARY_MODULE_FUNCTION
   );
I have checked UCBA1 and CS(clock system) registers on CCS debugger and they are both identical for those 2 MCUs. I cannot see any difference with the registers

I have tested UCB0 as I2C on pins P1.6 and P1.7 and it has the same result with no activity on pins.

I have also tested P1.4, P1.6 and P1.7 pins as GPIO output and toogle them with some delay. I can clearly see the activity on oscilloscope. I am sure that chip is soldered well and measuring points are connected to chip.
When I set pins as GPIO they are ok but I cannot set them as SPI or I2C. Please help to solve the issue.

#include <msp430.h>
#include <driverlib.h>
//#include "I2CMaster.h"

uint8_t TXData;
uint8_t RXData;


void delayMs(int ms){
    int i;
    while(ms--){
        i = 1000;
        while(i--);
    }
}

int main(void)
{
	WDTCTL = WDTPW | WDTHOLD;	// stop watchdog timer

    //Set DCO frequency to max DCO setting
    CS_setDCOFreq(CS_DCORSEL_0,CS_DCOFSEL_6); // dco @8mhz
//    CS_setDCOFreq(CS_DCORSEL_0,CS_DCOFSEL_3);
    //Select DCO as the clock source for SMCLK with no frequency divider
    CS_initClockSignal(CS_SMCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);
    CS_initClockSignal(CS_MCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);

    GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0);
    //GPIO test init
//    GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN4|GPIO_PIN6| GPIO_PIN7);

   GPIO_setAsPeripheralModuleFunctionInputPin(
       GPIO_PORT_P1,
       GPIO_PIN4 + GPIO_PIN6 + GPIO_PIN7,
       GPIO_SECONDARY_MODULE_FUNCTION
   );

   PMM_unlockLPM5();
//
//   //Initialize Master
   EUSCI_B_SPI_initMasterParam param = {0};
   param.selectClockSource = EUSCI_B_SPI_CLOCKSOURCE_SMCLK;
   param.clockSourceFrequency = CS_getSMCLK();
   param.desiredSpiClock = 500000;
   param.msbFirst = EUSCI_B_SPI_MSB_FIRST;
   param.clockPhase = EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT;
   param.clockPolarity = EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH;
   param.spiMode = EUSCI_B_SPI_3PIN;

   EUSCI_B_SPI_initMaster(EUSCI_B0_BASE, &param);
   EUSCI_B_SPI_enable(EUSCI_B0_BASE);
   EUSCI_B_SPI_clearInterrupt(EUSCI_B0_BASE,
           EUSCI_B_SPI_RECEIVE_INTERRUPT);
   // Enable USCI_B0 RX interrupt
   EUSCI_B_SPI_enableInterrupt(EUSCI_B0_BASE,
       EUSCI_B_SPI_RECEIVE_INTERRUPT);
   __delay_cycles(200);

   TXData = 0x55;                             // Holds TX data

	while(1){

	     while (!EUSCI_B_SPI_getInterruptStatus(EUSCI_B0_BASE,
	             EUSCI_B_SPI_TRANSMIT_INTERRUPT)) ;
         //Transmit Data to slave
         EUSCI_B_SPI_transmitData(EUSCI_B0_BASE, TXData);

	     GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
//	     GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN4 + GPIO_PIN6 + GPIO_PIN7);
	     delayMs(50);
	     GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
//	     GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN4 + GPIO_PIN6 + GPIO_PIN7);
         delayMs(50);
	}

	return 0;
}


__attribute__((interrupt(USCI_B0_VECTOR))) void USCI_B0_ISR (void)
{
    switch (__even_in_range(UCB0IV, USCI_SPI_UCTXIFG))
    {
        case USCI_SPI_UCRXIFG:      // UCRXIFG
            //USCI_B0 TX buffer ready?
            while (!EUSCI_B_SPI_getInterruptStatus(EUSCI_B0_BASE,
                        EUSCI_B_SPI_TRANSMIT_INTERRUPT));

            RXData = EUSCI_B_SPI_receiveData(EUSCI_B0_BASE);

            //Increment data
//            TXData++;

            //Send next value
//            EUSCI_B_SPI_transmitData(EUSCI_B0_BASE,
//                TXData
//                );

            //Delay between transmissions for slave to process information
            __delay_cycles(40);
            break;
        default:
            break;
    }
}

**Attention** This is a public forum