Part Number: MSP430FR2355
Hello team,
I want to send RTC along with 100bytes of data from one msp430fr2355 to other msp430fr2355 through UART.
Now need to capture the RTC at last byte in first msp430 and again capture RTC at first byte reception in second msp430. finally i want to know time taken to receive first and last byte to second msp430. Can anyone help me to implement this would be very thankful. below is the RTC code
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P2SEL1 |= BIT6 | BIT7; // P2.6~P2.7: crystal pins
do
{
CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1 & OFIFG); // Test oscillator fault flag
P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state
P1DIR |= BIT0; // Set P1.0 to output direction
PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate previously configured port settings
// RTC count re-load compare value at 32.
// 1024/32768 * 32 = 1 sec.
RTCMOD = 32-1;
// Initialize RTC
// Source = 32kHz crystal, divided by 1024
RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024 | RTCIE;
__bis_SR_register(LPM3_bits | GIE); // Enter LPM3, enable interrupt
}
// RTC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=RTC_VECTOR
__interrupt void RTC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(RTCIV,RTCIV_RTCIF))
{
case RTCIV_NONE: break; // No interrupt
case RTCIV_RTCIF: // RTC Overflow
P1OUT ^= BIT0;
rtc++; ////// i need to send this rtc(unsigned long int) value to next msp430.
break;
default: break;
}
}