How to enhance the detection distance of ESI module to metal? What aspects should we start from?Which parameters to modify in the code
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to enhance the detection distance of ESI module to metal? What aspects should we start from?Which parameters to modify in the code
Please wait for some time. I need to refer to our colleague about this problem.
Hi,
I want to check with you on the following items,
1. What is the target distance? What is the distance you get now?
2. Are you using 2LC or 3LC sensors? What is the part number of the L you are using now?
3. What is the size of your metal disk? What material does the metal disk made of?
Best regards,
Cash Hao
Hi,
1.The target range was 5.8mm, so far 4.8mm has been achieved
2.Use the 3LC scheme.L=470uH,C=220pF.Vcc=3V
3.Diameter 13mm, the material is stainless steel
thank you.
Hi,
Some things you can try with. It should be helpful.
1. Try to use a larger L. Like 1mH or 1.5mH.
2. Place the L on the edge of the metal disk.
Best regards,
Cash Hao
Hi,
How to choose the capacitance, high frequency or low good.
In addition, how to lengthen the oscillation time of LC in the program? The lengthening of the oscillation time should be able to adapt to a longer distance
thanks
Hi,
It doesn't necessary to change the capacitance, 220pF should work. High frequency is better.
You can change the TSM settings to get a longer oscillation time. However, I don't think it will help to get a longer distance.
Best regards,
Cash Hao
According to your suggestion, I changed the inductance of 1mH and the capacitor of 220pF, and now the rotation speed is correctly collected at the room temperature with a distance of 5.3mm.But it misses counting at 60 degrees Celsius.What parameters do you want to change now
Hi,
When the temperature changes, the L is going to change. That means the TSM settings will not detecting at the right time. You may need recalibration the TSM and DAC value. Or you can choose a L which less sensitive to temperature.
Best regards,
Cash Hao
**Attention** This is a public forum