Using the MSP-EXP430F5529 LaunchPad (red, rev 1.8)
Downloaded several UART program examples from Resource Explorer:
MSP430F55xx_uscia0_uart_01.c
MSP430F55xx_uscia0_uart_02.c
Both do a loopback test on pins listed below, put a jumper across these to connect them (also tried without the jumper)
P3.3 USCI_A0 Tx
P3.4 USCI_A0 Rx
Using a PC terminal emulator: Tera Term, Putty, CCS Terminal; get port address from Device Manager after LP connected with USB cable
Port settings for terminal & port are identical and match what each program wants
Tera Term set to local echo so I can see what I type, but there is no return of the same character, why not?