This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to connect display like this:
http://www.sharpmemorylcd.com/1-35-inch-memory-lcd.html
to the EZ430-Chronos?
Alexey
Aleksey,
The display you are pointing to seems to have a SPI interface and a few other GPIO lines. If these are available in the EZ430-Chronos, or you disconnect something to make them available, then you will be able to use it.
Gustavo
Sort of. All LCD-related port pins of any MSP can be alternatively used as plain digital general-purpose I/O. And so are the lines on the LCD_Bottom bus.Aleksey said:Will it be possible to use LCD_Bottom bus?
I doubt, however, that one of these lines is multiplexted with the signals from the hardware SPI/I2C interface. So you'll either do the interfacing with software bit-banging, or you'll need to re-route some signals from other pins. The datasheet of the msp430F6137 will tell you more.
Jens-Michael Gross said:The datasheet of the msp430F6137 will tell you more.
Can you give me a link to it?
I need something like here
http://www.sharpmemorylcd.com/resources/LS013B4DN02_Application_Info.pdf
There are a lot of things, voltage, power consumption, description of pins, etc.
Can TI provide me with the similar information about the current display of EZ430-Chronos so I could be sure that it is possible to attach new display?
**Attention** This is a public forum