This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a way to verify entry to the BSL mode for this device.
I have used the hardware entry sequence as indicated on page 6 of SLAU550W, figure 2
I am using a 3.3V supply voltage.
I have not been able to detect any activity on the BSL Data transmit ( P1.7 ).
Can anyone help me out?
Thanks
Frank Mimick
Hi
Yes, you can send a byte not equal to 0x80 to MSP430, if it is in BSL mode it will return 0x51 if not there is no information there.
**Attention** This is a public forum