Hello,
I am using CCS 4.2 with a custom board (MSP430F1612) .The board has an external watchdog connected to reset line of the MCU and additional line tied to one of the IO pin for preventing resetting the MCU, beside this there are no control lines over WDT from MCU.
When attempt to download the software to the MCU the CCS returns an error. Target is shown as suspended and during the program download an error "Cannot write to target" appears.
When using IAR with the same board , a dialog presented with a retry option once the reset occurs and then the download process continues. (The debug of course is not possible but download succeeds).
Please your advice regarding the CCS or other options to download the program.
I tried the lite version of elpotronics, the gang programmer - all of them have the same result, either they could not connect to the target or the flashing halted in the middle.
Thanks.