I need to use the Bootstrap Loader (BSL) functionality to field-program the MSP430F2330, however I need to use the standard UART port (on P3.4/P3.5) for the serial interface, not the factory BSL P1.1 and P2.2.
- Can the 'F2330 factory BSL be replaced with a custom BSL?
- If it can be replaced, is there a sample project for an 'F2330 BSL that uses the standard UART peripheral (CCS version preferred)?
- I need to enter the BSL via a jump/call from my own application code.
- If the factory BSL cannot be replaced, can I just merge a custom version of the BSL code with my own application code?
- If so, I would just call the custom BSL code and ignore the factory BSL
- Again, is there a sample project for an 'F2330 BSL that uses the standard UART peripheral (CCS version preferred)?
Thanks,
Ron