This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET430UIF stops working today



I have been using the MSP-FET430UIF successfully for months to program an MSP430. I have set up two computers to do programming, each with a dedicated MSP-FET430UIF debugger. Last Friday I was setting up a third PC as an additional programming station. In the middle of the IAR Kickstart install, I was asked to upgrade the firmware in my debugger. I clicked OK. Now I get the error "Fatal error: Failed to initialize.  Check if hardware is connected. Check if drivers are installed. Try to restart the computer. Tools using the parallel port are not supported on Windows Vista   Session aborted! " It also says "Failed to load flash loader: C:\testproject.d43" I have Windows 7 and IAR Embedded Workbench Kickstart for MSP430 5.30.4. I have tried three installs of IAR, three different degugger units, and two different target boards. How can I get IAR Kickstart and the debuggers back into production? I don't know where to start.

**Attention** This is a public forum