This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

converting a big project from IAR to CCS - how?



I would like to inquire if there are any automated tools, scripts or recommended practices for converting a fairly large and complex IAR project for a CC430 to CCS? It seems the "Import" function in CCS doesn't provide a path for such a migration, sadly. 

Thanks in advance for any advice,

-r

  • Porting from one toolset to an entirely different one is never simple.

    I don't know of any automated tools; it would obviously not be in IAR's interest to provide such a thing, and probably wouldn't be worth the effort for TI (and they might be mindful of their relationship with IAR, anyhow...)

    Porting requires a thorough understand of both the original toolset and the new toolset - so a lot of study of manuals is, I'm afraid, unavoidable.

    As a start, I would check your IAR documentation to see if there is an option to disable all its extensions and special features - then use this to get your code to a point where it is "pure ANSI". You should then, at least, be able to get it to compile on another toolset.

    Then there's the question of your source code: has it been carefully written to be portable - or is it deeply entwined with IAR-specifics?

    If the code is not carefully written to be portable,  it may be better to start by making it portable in IAR, and then moving the result to CCS...

     

  • Thanks for the quick response. My code doesn't use any IAR specifics and is almost all pure ANSI C, so i was more wondering about how to convert project settings from IAR to CCS.

  • Rene Limberger said:
    how to convert project settings from IAR to CCS.

    This is where "a thorough understand of both the original toolset and the new toolset " comes in!

    • You need a thorough understand of IAR in order to be sure of what all the current settings do;
    • You need a thorough understand of CCS in order to know how to achieve those same things in CCS.

    I think you're just going to have to go through each setting in each dialogue, and convert each one over to CCS.

    A fundamental flaw with all GUI IDEs that I've ever used is getting them to produce a full listing of all the sttings used. It usually just comes down to taking screenshots of the dialogues!

    Usually, compiler listing files show the active option settings - so that might help you...

     

**Attention** This is a public forum