Other Parts Discussed in Thread: MSP430F5510
Hi,
I'm trying to run example application for USB communication. 12 MHz crystal is used as XT2 oscillator. I copied C1_Eample folder form TI USB Developers Pack. I changed device to MSP430f5510, USB_MCLK_FREQ to 12000000 and USB_XT_FREQ to USBPLL_SETCLK_12_0.
Building all, debuging, running.
When I connect usb port to PC, Windows (7, x64) the device manager shows "Unknow Device". After checking its proporties I see something like this (this is not my picture, but device status is the same):
After uninstalling existing drivers and installing new ones choosing folder with .inf file I have (now it is my screen):
In proporties I can see Code 10 error. Of course there isn' t COM4 in terminal.
Directly choosing .inf file as an installation file occurs message the file isn't proper for this system, but if we open .inf file in Wordpad we can see section: for Windows x64.
Maybe isn't it supported by Windows 7?
Has anyone any idea what is wrong?
Regards,
Mikolaj