I'm using a an MSP430F5506 microcontroller and I am having some problems running my code repeatedly. I do not have any problem debugging my code and I know it is running on my device because the LEDs are blinking when they are supposed to. The problem is that when I take the debugger off the code will not run anymore and I am presuming that it was not saved into flash correctly. Has anyone seen this before? I am using the MSP430-FETUIF with SPY-bi-Wire if that helps.