Hi All
I am using the MSP430 USB-Debug-Interface 'MSP-FET430UIF' (V1.4a) and the Target Board 'MSP-TS430PW24' (Rev 1.0) provided with the device MSP430AFE253.
When I have built my project I cannot connect the target with the debugger of the 'Code Composer Studio' (5.3.0). If I click DEBUG on the toolbar a window opens with following message: "Error connecting to the target: Unknown device".
In my CCS project folder there are the following device-related files: 'lnk_msp430afe253.cmd' and 'MSP430AFE253.ccxml' [Active] in subfolder 'targetConfigs'.
I have tried to connect the target by JTAG and Spy-Bi-Wire but all trials failed.
I am not so familiar with MSP430 and CCS. Does anyone have an idea to help me?
Thanks
Guenther