I am using MSP430G2553 on my custom board. Attached is my circuit.
I have below queries:
Oscillator selection:
I have to operate my system on 16Mhz external oscillator.
1. I have selected this oscillator with load capacitance of 12pF:
EDIT: http://www.digikey.com/product-detail/en/AA-16.000MALE-T/887-1660-2-ND/3454676
What should be value of capacitor I connect. Is it two 12pF capacitors?
2. Launchpad of G series also have zero ohm resistors connected across XIN & XOut. Do I need to connect some value resistors also or crystal with 2 load capacitor will work fine.
Debug:
1. Since I am working on my custom board , can I pick jumper wires from launchpad to debug my IC on custom board.
I am already using rxd & txd for uart. So I have left with TEST,RESET & GND.
So I make all jumper on connector J3 of launchpad pad open & then pick three wires TEST,RESET & GND from launchpad & then try todebug my custom board. Will it work.?
2. If not do I need to buy additional debugger from TI?
Open Pins:
1. On user guide of MSP430G2553 ( SLAU144J), Page 41 shows that reset should have less than 2.2nF capacitor if Spy bi interface is selected. & 10nF otherwise.
Does that mean once my program is final I have to repalce that capacitor in the end before sending to filed.
2. Test pin I have left open. Is it ok?
Information memory:
1. Can I use information memory as eeprom. In filed this device has to be calibrated several times. So can I read/write the data & read data on start up?