Hello,
I´ve a board TS430PM64A and using a MSP430f249 on socket.
I try to use JTag supply / external power supply and my jtag MSP-FET430UIF don´t work.
Using other development board SoftBaught ES1611 it´s ok!
I´ve power supply ok, Jumper with correct configuration, but my JTag isn´t work with this hardware.
I´m using a code sample at CCS v5 90 days
Error message:
MSP430: Can't Initialize Target CPU: **Error**: Serial Communication failed at port: COM3, baud rate:9600! To use serial monitor, please ensure the following prerequisites are satisfied: 1. Make sure the cable is plugged into both the target and the host on the right COM port. 2. Make sure a compatible target side serial monitor is loaded and running on the target device.