Hi all,
I try to make FR6922 get into LPM4.5 mode, but it doesn't work. I measure the current consumption and find a fixed current pattern as show below. Please note there is a LCD connected but it is disabled by setting LCDCCTL0=0.
I design a current meter by using a high precision OPA with gain=100 and a 10ohm resistor. So, 1V = 1mA. The measured "CH1 Mean" is 29.39mV --> 29.39uA. The frequency of the measured pattern is about 430~470Hz. I guess there is a module still working inside FR6922.
Does any one know the reason?