Part Number: MSP430FR6989
Hi,
Im a newbie to MSP430 Programming. Im currently working on MSP430FR6989 LaunchPad board. I would like to sample 3 ADC input channels repeatedly. After going through the Datasheet,User Guide and sample programs, i wrote the below code to sample analog inputs from A3(P1.3),A4(P8.7) and A5(P8.6).
My expected behaviour for the below code is The ADC12 should convert MEM0(no interrupt),MEM1(no interrupt) and MEM2(Generate Interrupt) where in the ADC ISR Routine i will copy the register contents from MEM0,1 and 2 to the global variables.By this way, the sequence of sampling and interrupt shall continue to occur. The problem i face here is, the interrupt is not generated when i set the value ADC12IER0 |= ADC12IE2( i.e at end of seq ). Whereas when i change the value to ADC12IER0 |= ADC12IE0, the interrupt is generated for MEM0 and channel A3 is alone sampled. Below is the code. Requesting your kind guidance here friends. Thank you in advance.
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1SEL1 |= BIT3; // Configure P1.3 for ADC
P1SEL0 |= BIT3;
P8SEL1 |= BIT6; // Configure P8.6 for ADC
P8SEL0 |= BIT6;
P8SEL1 |= BIT7; // Configure P8.7 for ADC
P8SEL0 |= BIT7;
PM5CTL0 &= ~LOCKLPM5;
while(REFCTL0 & REFGENBUSY);
REFCTL0 |= REFVSEL_3 | REFON;
// Configure ADC12
ADC12CTL0 = ADC12SHT0_2 | ADC12ON;
ADC12CTL1 = ADC12SHP| ADC12CONSEQ_2;
ADC12CTL2 &= 0xCF; // 8-bit resolution
ADC12IER0 |= ADC12IE2; //Generate Interrupt for MEM2 ADC Data load
ADC12MCTL0 |= ADC12INCH_3; // A3 chan
ADC12MCTL0 |= ADC12VRSEL_1; //Vref = 2.5V
ADC12MCTL1 |= ADC12INCH_4;// A4 chan
ADC12MCTL1 |= ADC12VRSEL_1;//Vref = 2.5V
ADC12MCTL2 |= ADC12INCH_5+ADC12EOS;// A5 chan , End of Sequence
ADC12MCTL2 |= ADC12VRSEL_1;//Vref = 2.5V
while(1)
{
__delay_cycles(5000); // Delay between conversions
ADC12CTL0 |= ADC12ENC | ADC12SC; // Sampling and conversion start
__no_operation(); // For debug only
}
}
#pragma vector = ADC12_VECTOR
__interrupt void ADC12_ISR(void)
#endif
{
switch (__even_in_range(ADC12IV, ADC12IV_ADC12RDYIFG))
{
case ADC12IV_NONE: break; // Vector 0: No interrupt
case ADC12IV_ADC12OVIFG: break; // Vector 2: ADC12MEMx Overflow
case ADC12IV_ADC12TOVIFG: break; // Vector 4: Conversion time overflow
case ADC12IV_ADC12HIIFG: break; // Vector 6: ADC12BHI
case ADC12IV_ADC12LOIFG: break; // Vector 8: ADC12BLO
case ADC12IV_ADC12INIFG: break; // Vector 10: ADC12BIN
case ADC12IV_ADC12IFG0: break; // Vector 12: ADC12MEM0 Interrupt
case ADC12IV_ADC12IFG1: break; // Vector 14: ADC12MEM1
case ADC12IV_ADC12IFG2: // Vector 16: ADC12MEM2
ADCValue0 = ADC12MEM0;
ADCValue1 = ADC12MEM1;
ADCValue2 = ADC12MEM2;
break;
case ADC12IV_ADC12IFG3: break;
case ADC12IV_ADC12IFG4: break; // Vector 20: ADC12MEM4
case ADC12IV_ADC12IFG5: break; // Vector 22: ADC12MEM5
case ADC12IV_ADC12IFG6: break; // Vector 24: ADC12MEM6
case ADC12IV_ADC12IFG7: break; // Vector 26: ADC12MEM7
case ADC12IV_ADC12IFG8: break; // Vector 28: ADC12MEM8
case ADC12IV_ADC12IFG9: break; // Vector 30: ADC12MEM9
.........
}