Other Parts Discussed in Thread: MSP432WARE
The code for the example "adc_14_single_channel_temperature_sensor" in version 3.21.00.05 of the driver library has a few problems. The original code for the interrupt handler is:
void ADC14_IRQHandler(void)
{
uint64_t status;
uint32_t cal30, cal85;
status = ADC14_getEnabledInterruptStatus();
ADC14_clearInterruptFlag(status);
if(status & ADC_INT0)
{
cal30 = SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,
SYSCTL_30_DEGREES_C);
cal85 = SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,
SYSCTL_85_DEGREES_C);
tempC = (float) (((uint32_t) ADC14_getResult(ADC_MEM0) - cal30) * (85 - 30))
/ (cal85 - cal30) + 30.0f;
tempF = tempC * 9.0f / 5.0f + 32.0f;
}
}
When I run the unmodified example on my version 2 MSP432 Launchpad, I get a temperature reading of 5.76 million degrees C. Seems a little hot. The problem is that the results from the adc are smaller than cal30. Since the variables are uin32_t, subtracting cal30 gives a huge positive number rather than a negative number. Changing the types to int32_t does the calculation correctly. However, I am still not getting a reasonable temperature. The values are:
cal30 = 4881
cal85 = 5626
ADC14_getResult returns (3638 or a number close to that)
This gives -61.77 deg C. So either the calibration constants are wrong or there is something wrong with the way the example is reading the adc.
Update: I found from another forum entry that there is a bug in the adc setup. The line:
ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_AVCC_VREFNEG_VSS, ADC_INPUT_A22, false);
should be
ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_INTBUF_VREFNEG_VSS, ADC_INPUT_A22, false);
Now the result is 25.7 deg C, which is reasonable.
Also, when I run the code on my version 1 MSP432 Launchpad, I get a divide by zero error. That is because cal30 and cal85 are both defined as 0xffff on the XMS432 Rev B processor that I have, so the denominator (cal85 - cal30) is zero. The code should check for that.
The interrupt routine that I am now using is:
void ADC14_IRQHandler(void)
{
uint64_t status;
int32_t cal30, cal85, adcval, denom;
status = ADC14_getEnabledInterruptStatus();
ADC14_clearInterruptFlag(status);
if(status & ADC_INT0)
{
cal30 = SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,
SYSCTL_30_DEGREES_C);
cal85 = SysCtl_getTempCalibrationConstant(SYSCTL_2_5V_REF,
SYSCTL_85_DEGREES_C);
adcval = (int32_t) ADC14_getResult(ADC_MEM0);
denom = (cal85 - cal30);
if (denom != 0)
tempC = (float) ((adcval - cal30) * (85 - 30))
/ denom + 30.0f;
else
tempC = -40.0f;
tempF = tempC * 9.0f / 5.0f + 32.0f;
}
}
Along with the change to ADC14_configureConversionMemory, this seems to solve the problems.