Hi,
I just upgraded the MSP432E401Y SimpleLink SDK from version 2.30.00.14 to version 2.40.00.11. My application has a thread that periodically makes HTTPClient requests via my wired ethernet connection. Prior to the upgrade I had no problems sending requests or receiving responses from my web service and the thread runs stable. Since the upgrade and running the exact same baseline of my software, the thread runs for a few seconds then the HTTPClient_connect() fails with a -10 error code. If I switch back to version 2.30.00.14 and rebuild, all works fine. I checked the release notes for version 2.40.00.11 and did not see anything that would impact the HTTPClient interface. I am using Code Composer Studio v8.2.0.00007. Any ideas on why this is happening?
Thanks,
Tim