Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi,
I am studying about the algorithm of voice recognition and I noticed that in the display when a record of a phrase appears the status of the enroll of a number that I did not understand what it means and another number that according to the library says to be the quality of the audio.
I have some doubts. The first is why the VCD_getEnrollQuality (VCD_handle, & quality) function always returns in the variable quality always the value 32767 (in debug), and in the comments of this function says that the value always stays between 0 and 1 ?.
How to understand the quality parameter displayed on the display, in all the tests I did always display "10", is this the highest quality ?.
Another point I wanted to address is what the number displayed before the quality parameters means, it's a number I did not understand what that means, sometimes it appears as 136, 164 and other values. What does this number say?.
Regards,
Leonardo!