Tool/software: Code Composer Studio
Hi,
I have manually imported the MSP-EXP432P401R_GrlibExample project into CCS V9.0.1.00004. I have resolved all the missing include files and so on but I'm stuck with these missing symbols. Will someone please help me sort out this (I hope final) piece of the puzzle? They seem to be somehow intrinsic but don't seem to be in any file that I can find. This is my first attempt to do anything with an MSP432Pxxx family part, having used MSP430 parts up until now.
undefined first referenced
symbol in file
--------- ----------------
CS_getSMCLK ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
CS_initClockSignal ./main.obj
CS_setDCOCenteredFrequency ./main.obj
CS_setDCOFrequency ./main.obj
FPU_enableModule ./main.obj
FlashCtl_setWaitState ./main.obj
GPIO_setAsOutputPin ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
GPIO_setAsPeripheralModuleFunctionOutputPin ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
GPIO_setOutputHighOnPin ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
GPIO_setOutputLowOnPin ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
PCM_setPowerState ./main.obj
SPI_clearInterruptFlag ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
SPI_enableModule ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
SPI_getInterruptStatus ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
SPI_initMaster ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
SPI_isBusy ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
SPI_transmitData ./LcdDriver/HAL_MSP_EXP432P401R_KITRONIX320X240_SSD2119_SPI.obj
WDT_A_holdTimer ./main.obj
g_sFontCm18 ./main.obj
g_sFontCmss20b ./main.obj
error #10234-D: unresolved symbols remain
Cheers, John L.