Hi Sir,
I tries to used MSP430F5438A UART BSL scripter read specified address data.
First time, I read the data, it is correct. the log file as below
script_543x_uart_read_data_2019May21_111756.log
--------------------------------------------------------- BSL Scripter 3.4.0.1 PC software for BSL programming 2019-May-21 11:17:56 --------------------------------------------------------- Input file script is : C:/ti/bsl-scripter-windows/script_543x_uart_read_data.txt MODE msp430f5xx UART COM3 DELAY 1000 Delay 1000 ms VERBOSE Verbose mode is now on! DELAY 1000 Delay 1000 ms //MASS_ERASE //RX_PASSWORD .\pass16_default.txt RX_PASSWORD [80] [21] [00] [11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [9e] [e6] <80> <02> <00> <3b> <00> <60> <c4> BSL Password is correct! //RX_DATA_BLOCK .\blinkLED_f5438.txt DELAY 1000 Delay 1000 ms TX_DATA_BLOCK 0x5C00 0x1F Data_Read.txt Write Txt File : C:/ti/bsl-scripter-windows/Data_Read.txt [80] [06] [00] [18] [00] [5c] [00] [1f] [00] [92] [30] <80> <20> <00> <3a> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <ff> <1e> <3c> Time elapsed of reading 31 bytes : 0.1349 seconds Speed of reading data : 0.2244(kB/s) DELAY 1000 Delay 1000 ms SET_PC 0x5c00 [80] [04] [00] [17] [00] [5c] [00] [98] [85]
The second time, I read the data again, it is unable to read. the log file as below
script_543x_uart_read_data_2019May21_111811.log
--------------------------------------------------------- BSL Scripter 3.4.0.1 PC software for BSL programming 2019-May-21 11:18:11 --------------------------------------------------------- Input file script is : C:/ti/bsl-scripter-windows/script_543x_uart_read_data.txt MODE msp430f5xx UART COM3 DELAY 1000 Delay 1000 ms VERBOSE Verbose mode is now on! DELAY 1000 Delay 1000 ms //MASS_ERASE //RX_PASSWORD .\pass16_default.txt RX_PASSWORD [80] [21] [00] [11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [9e] [e6] <00> <80> <02> //RX_DATA_BLOCK .\blinkLED_f5438.txt DELAY 1000 Delay 1000 ms TX_DATA_BLOCK 0x5C00 0x1F Data_Read.txt Write Txt File : C:/ti/bsl-scripter-windows/Data_Read.txt Time elapsed of reading 0 bytes : 0.01099 seconds Speed of reading data : 0(kB/s) DELAY 1000 Delay 1000 ms SET_PC 0x5c00 [80] [04] [00] [17] [00] [5c] [00] [98] [85]
Would you know why can I only read once???