I'm using IAR and FET430UIF V1.4a, firmware updated by IAR 7.12.3. FR5994 is selected in the project options. ( I have also tried EZ-msp2013 as an FET. Not sure if that should be expected to work talking to an FR59xx target.)
This is embarrassing. It smells like some kind of rookie mistake.
I can successfully talk to the 80-pin PN-packaged FZ5994 on its launch pad, which uses Spy BiWire, but have been unsuccessful in using SBW talking to any of my own targets that use the 48-pin RGZ package. Obvious, right? Mis-wired! Except I have checked it every way I can and it seems ok: Pin 1 of the JTAG connector to pin 23 of the processor (RST/SBWTDIO) and pin 7 of the JTAG to pin 22 (TEST/SBWTCK). Power and ground, of course and the voltmeter says I have power. Ohmmeter says the right pins are connected together and neither net is to grounded. I made up a socket board for loose chips and a probe fixture for my prototypes with their soldered chips. Neither will respond. IAR says none found or unsupported. I have ordered fresh processors and contacted them in the socket board, inserting with static precautions, in case I had killed the earlier ones with static or soldering. Always the same message.
The errata sheet lists no debug issues.
SO, is there any sort of known trap waiting for the unwary when using the RGZ package with SBW?