Other Parts Discussed in Thread: MSP430WARE
Tool/software: Code Composer Studio
Happy New Years TI Team,
I have a small issue I would like to get some guidance. I'm using the MSP430FR6989 LaunchPad development kit. I am completing the MSP430 Workshop tutorial Booklet which is very good. The workshop does not mention the FR6989, I suspect the device was not released at the time of writing this workshop. Nevertheless things are going very well - for the workshop I have been following the flow for the FR5969.
Presently I am completing Chapter 5 "Interrupts", actually on the last page of this chapter where there is an optional LAB called Lab 5b on page 5-53.
This lab requires a download from the TI Resource Explorer. The download is actually a CCS project IMPORT called "wdt_a_ex2_intervalACLK". This example uses WDT as a standard timer for causing an internal INTERRUPT.
I wish to complete this Optional Lab 5b but TI Resource Explorer does not seem to have this EXAMPLE PROJECT as defined in the workbook.
My question, is this EXAMPLE PROJECT LAB 5b for MSP430 Workshop done only for the FR5969 and not the FR6989?
If so, I would appreciate if anyone can point out the location for the FR6989 and this lab.
Thanks