Other Parts Discussed in Thread: LDC1314, , SN74LV1T125, MSP430L092
Tool/software: TI C/C++ Compiler
Dears
We use MSP430FR2433 connect to LDC1314 with I2C interface.
1. USE external oscillator connect to MSP430FR2433 P1.6 and P1.0 as timer TA0.CCI1A and TA1.CC12A.
2. MSP430FR2433 worked at 2.8V.
3. external oscillator signal's voltage amplitude which input to MSP430FR2433's P1.0/P1.6 is 1V. My question is MSP430FR2433 can't detect the oscillator signal since Voltage amplitude is only 1V.
because we are low power solution, there's no room space to increase oscillator signal Voltage amplitude. Is there anyway to configure MSP430FR2433 or change schematics so that MSP430FR2433
timer can detect the 1V amplitude oscillator input signal? Even with schematics changed ,we hope it's sill low power.
thanks a lot and best regards