Part Number: MSP-EXP432P401R
Hello, i have recently gotten two MSP-EXP432P401R development boards and neither of them are able to be flashed too. Code composer comes up with:
This error is generated by TI's USCIF driver or utilities.
The value is '-591' (0xfffffdb1).
The title is 'SC_ERR_AUTO110_DFU_OPEN'.
The explanation is:
The firmware updater encountered an error and could not finish. The
updater failed to connect to the XDS110 in programming mode. Unplug
and re-plug the XDS110, and try again. If the problem remains, try
updating the firmware using the xdsdfu utility found in the
.../ccs_base/common/uscif/xds110 directory of the installation.
View the XDS110SupportReadMe.pdf file there for instructions.
so i went and used the xdsdfu software and it seems to be an issue with it going into DFU mode, whenever i do this the device appears to turn into a "Tiva Device Firmware Update" with the serial number of 00000000 and is not detected by the xdsdfu software.
I have tried both devices with every USB connector i could find and on all usb ports on my machine. Any help will be greatly appreciated.
My system is:
OS: Ubuntu 18.04
Code Composer: 10.0.0.00010