Hi,
My customer is using MSP430FR2433 and evaluate an internal temp sensor.
He uses calibration values stored in TLV (address 1A1Ah / 1A1Ch).
According to datasheet, these calibration values are 30+/-3C and 85+/-3C.
But he found some devices shows much more errors.
Please see attached excel.
MSP430_temp.xlsx
5 samples were tested.
Column B is device case temperature.
Column C/D are counts number measured by the internal temp sensor.
Column E/F are calibration values stored in TLV for each sample.
Column G is calibrated temperature calculated by below formula:
IntDegC = (temp-CALADC_15V_30C)*(85-30)/(CALADC_15V_85C-CALADC_15V_30C)+30
As you can see, some values calculated are over +/-3C (in Red).
Especially sample#74 shows +10C at 30C and +5C at 85C.
Is this expected?
Thanks and regards,
Koichiro Tashiro