I got the LCD dev kit, played with it, wrote my first application for fr5969. CCS 5.5 prompted me to update the firmware I click go and now the board doesn't show up on the device manager.
I'm thinking I can JTAG's from from one of my 2 board stellaris CAN dev kits. But I would think that allow me to use the fr5969 without the very nice virtual serial port usb, etc.