Hello,
I've seen a couple of host-side code samples for updating MSP430 using the bootloader via UART, but not for i2c. Can someone point me to an i2c example?
Thanks, Hector
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I've seen a couple of host-side code samples for updating MSP430 using the bootloader via UART, but not for i2c. Can someone point me to an i2c example?
Thanks, Hector
I'm using the MSP430 FR2632 and trying to get it in BSL mode using the entry sequence with RST and TEST pins. I checked with the analyzer and the sequence looks correct as described in section 3.3.2 in doc SLAU550P. I'm attaching the analyzer output. Does the sequence look ok to you as well?
Also, I noticed that in SLAU550P, the FR2632 is not explicitly listed in table 1 in section 2. Is this a problem?
**Attention** This is a public forum