This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F2617: Initialising Digital I/O ports on lower pin count devices?

Part Number: MSP430F2617

Tool/software: Code Composer Studio

The MSP430F241x and 261x are available in 64 or 80 pin packages.

In the 64-pin variants, Digital I/O ports P7 and P8 are not implemented.

When compiling code for these lower pin count devices, CCS Low Power Advisor complains that P7 and P8 have not been initialised.

Is it advisable (or even possible) to initialise these ports and set them to output mode?

Thanks - Ray

**Attention** This is a public forum