HI,
I like to work in MSP430FR5969-SP so i have purchased a development board for it, in the development board high frequency oscillator is not available and in the schematics it is said as DNP,
i want to use the high frequency external crystal, but when i programmed for high frequency crystal , the crystal frequency cannot be viewed in oscilloscope, yet the microcontroller is not working as per the DCO frequency also as per the CTL2 register description
I have attached my sample program for clock, how do i enable external oscillator.
CSCTL0 = 0xA500;
CSCTL1 = 0x000C; /* 8 Mhz - 0x000C */
CSCTL2 = 0x0155; /* Aclk is VLOclk, SMclk & Mclk is HFXT clock */
CSCTL3 = 0x0000; /* crystal frequency is not divided */
CSCTL4 = 0x8881; /* SMclk on,LFxtclk off, HFXTCLK on , 4MHZ crystal selected */