Hello team,
I am working on an Non-Invasive and Non-Intrusive water flow meter.
I followed the first steps of the
https://www.ti.com/lit/ug/slau810b/slau810b.pdf?ts=1618936054234&ref_url=https%253A%252F%252Fdev.ti.com%252Ftirex%252Fexplore%252Fcontent%252Fmsp_academy_msp430_1_00_04_11%252Fmodules%252Fmsp430%252Fmsp430_uss_water_training%252Fmsp430_uss_water_training.html
I have pluged my ultrasonic transducers (1Mz) and I get the error
"No signal detected in up and downstream channel"
which also, is the same error when the transducers are unpluged.
As I can see in the forum, you suggest to soak the transducers. there is no way do test the system in another setup?
For now I just need to get some results without amplifications, see the correct wavesforms.
Best Regards
Manos