Other Parts Discussed in Thread: TM4C1294NCPDT, LMFLASHPROGRAMMER, UNIFLASH
Hi,
I'm using TM4C1294NCPDT with PoE on a custom board. I use the TI XDS100v2 USB debug probe to program the MCU.
I started the udpEcho sample (with a MAC address hardcoded in code), and everything worked fine. But one of the external PoE sources I use disables power when the debug probe is connected to the board. So I think the MCU got stuck in some transient state. (All voltage levels are correct so I suppose it wasn't damaged physically.)
I get the following error messages when I try to start debugging:
- CORTEX_M4_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.636.0)
CORTEX_M4_0: Flash Programmer: Timed out while writing to Flash memory
CORTEX_M4_0: GEL: File: - CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 0.0.0.0)
I'm using CCS6 on Windows. I can't even find how to "simple-reset" the device.
Can anyone please send me some instructions on how to (factory-) reset the device with these tools?
Thank you