Hi
Debug Probe Performance Comparison can be confirmed on
According to above site, TMDSEMU560V2STM is better than TMDSEMU200.
Q1) The frequency of JTAG TCLK of TMDSEMU560V2STM and TMDSEMU200 are same on above comparison?
Q2) Is the maximum frequency supported by TMDSEMU560V2STM and TMDSEMU200 the same?
Q3) What is the reason for the difference in performance betweenTMDSEMU560V2STM and TMDSEMU200 ?
(e.g. Max freq of them, or difference in performance between processors installed in the debug probe)
Thanks and Best regards,
HaTa.