This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A confusion in pre-define in TM4C c programing



Hello, Everybody. 

in TM4C c programming, There is "IntEnable( INT_TIMER0A )" operation,

Where, INT_TIMER0A is pre-defined like this:

#define INT_TIMER0A    INT_CONCAT( INT_TIMER0A_,  INT_DEVICE_CLASS)

and INT_CONCAT is defined as:

#define INT_CONCAT(intname, class)     INT_RESOLVE(intname, class)

and

#define INT_RESOLVE(intname, class)     intname##BLIZZARD

 

I just can not understand what is the function and purpose of "class" in these code. "class" is parameter in the definition, but why it does not function anything here? at least it seem so.

Thank you !