I am trying out usb_stick_update with usb_stick_demo with my TM4C1294XL Rev D launchpad
- The launchpad works fine other examples
- No problem in compiling the two projects
- Rename usb_stick_demo.bin to FIRMWARE.BIN
- Store FIRMWARE.BIN to the root directory of a 8GB SD card
- Insert the SD card to a card reader
- Connect the card reader to the target USB connector on Launchpad via a OTG USB cable
- Apply OTG jumper on JP1 to provide 5V to the USB connector on target (confirmed by reading 5V on TP4)
- When I debug usb_stick_update, I run into FaultISR
Instead of chasing the cause of this FaultISR, I would like to make sure my above steps are complete/enough to start the project
Thanks!