Part Number: BOOSTXL-DRV8320H
Other Parts Discussed in Thread: MSP430F5529, BOOSTXL-DRV8320S
Hi all,
A year ago I asked for advice to implement BLDC sensored control that meets the following characteristics:
* Nominal voltage of 24 Vdc.
* 10 amp rated current.
* Closed loop control (Hall sensors).
* External or internal speed control (not relevant).
* If the speed increases above the setting due to external conditions, the activated brake is reduced at the set point.
They advised me:
KIT BOOSTXL-DRV8320S + MSP430F5529
I was told that this solution has no speed loop and no active brake, but: "With that said, those features can be added into your system easily."
The system is working properly, except that I cannot maintain speed if the motor is revving from external causes.
Any suggestions on how to add those two functions to my system?
Many thanks
Gonzalo