This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear *,
which integrated driver would you recommend for the NEMA 34 Hybrid stepper motor 34HS1456 ?
https://cdn-reichelt.de/documents/datenblatt/X200/34HS1456.pdf
What yo you think about using DRV8412?
Best Regards,
D.
Hi Ryan,
thank you for the feedback. i like the idea to use DRV8711. I want to use it with a MSP MCU.
-Can you tell do you have a reference design recommendation that is close to the motor that we have ?-
does maybe TI have a sample source for MSP or other mcu for the DRV8711?
I see that the operating range of Driver is 8V to 52V, we are in the range of 12V to 48V input supply.
- are the 60V mosfets ok for the application or would you recommend the 100V mosfets?
- can yo maybe tell or suggest a application note on how to calculate the required input power for input power supply ?
Best Regards,
David.
David,
Reference design is here with software:
https://www.ti.com/tool/BOOST-DRV8711
60V is used on this reference design.
Power from power supply will depend mostly on the FETs that you choose and the loss in the FETs. You can calculate efficiency based on the Rdson of the FETs.
https://www.ti.com/lit/an/slyt664/slyt664.pdf
Regards,
Ryan