This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2604L: In closed loop mode, constant PWM drive is interrupted every 50 - 70 ms

Part Number: DRV2604L
Other Parts Discussed in Thread: DRV2605L

The attached screenshot shows the waveform of a PWM pulse lasting one second. (Pink is OUT+ and blue is OUT-)

This pulse is a constant PWM duty, but you can see that it is being interrupted by a number of drive signals from OUT-

This makes the motor sensation very jittery, not smooth. Why would it be doing this? How to fix it to be smooth?

(I know it could be switched to open-loop, but this loses features of the device such as braking.)