This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8870: Analysis of periodic fluctuation of motor current

Part Number: DRV8870

Hi all,

I'm a FAE of TI. When I tested with drv8870evm, I encountered a problem and wanted to get your answer.

When the motor is unloaded, we find that the motor current will fluctuate periodically. What is the reason? By providing 12V, 15V, 18V, 21V and 24V input voltages, we found that the current fluctuation period basically showed a positive proportional change. The test is as follows (there is an error in the interval between the two spikes)

12V:The frequency is approximately 362Hz.

15V:The frequency is approximately 423Hz.

18V:The frequency is approximately 510Hz.

21V:The frequency is approximately 510Hz.(There are errors here)

24V:The frequency is approximately 862Hz.

 

What causes this? How to verify?