Hi Team,
Our customer is looking for BLDC controllers for permanent magnet motor. According to our customer,
The back EMF of the motors range from 100-400V..but for now
If we can test controllers that can handle up to 150-160 Volts of back emf ..that would suffice…. The motor range from 8Nm to over 100Nm
Currently, we have a few BLDC motor drivers on stock, is the DRV8312, DRV8313 and DRV10982-Q1 suitable for these motors?
Regards,
Danilo