This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLDC controllers for permanent magnet motors

Other Parts Discussed in Thread: DRV10982-Q1, DRV8312, DRV8313, DRV8300

Hi Team,

Our customer is looking for BLDC controllers for permanent magnet motor. According to our customer,

The back EMF of the motors range from 100-400V..but for now

If we can test controllers that can handle up to 150-160 Volts of back emf ..that would suffice…. The motor range from 8Nm to over 100Nm

Currently, we have a few BLDC motor drivers on stock, is the DRV8312, DRV8313 and DRV10982-Q1 suitable for these motors?

Regards,

Danilo