Hello,
I am making camera stabilizator for camera for school project. I am first trying to just spin motors with drv10975. If I output 0 on speed pin, motor doesn't spin, which is correct, but after adding some voltage with potentiometer, motor firstly have some trouble to spin, then it slowly accelerate speed and at some point it just stops like in video: https://youtu.be/rfIJglZclI0 . It always does the same. I am using ESP32, 12V supply and motor with these specifications:
- Resistance: 5.57 Ω ± 5%
- Pre-wounded: with 130 turns, 3.17 mm shaft
- Camera range: 200 - 500 g
- Voltage: 12 V
- Current: 1 A
- RPM: 2149 ~ 2375
- Torque: 600 - 1000 g.cm
- Weight: 80.3 g
My circuit:
This is output betwen one phase and GND: https://youtu.be/iT7zRFGEIjU
Thanks for help.
Mitja