Other Parts Discussed in Thread: DRV8874
Hi Team,
My customer is using AT8236, which is a BDC driver with following spec, 4.5A peak current, 3 A continue current, Typical RDSon(HS + LS) is 200mΩ. Customers have found that the AT8236 gets very hot at 3A continuous current. Do you think DRV8251 with 450mΩ is a good P2P alternatives? How does the temperature rise of the DRV8251 perform under the condition of 3A continuous current? Or is there is any other options?
Thanks and best regards,
Hailiang